2023-05-25 11:48 PM
I am using TouchGFX 4.20.0 library. We are storing all the Fonts and images to the external memory. During the initialization as per the selected language we are caching the respected Fonts and successfully load the fonts and able to see correct text. We also cache all the images upfront. But while our display module is receiving large number of CAN messages on the CAN task sometimes we observed the few texts on the screen becomes garbled. The issue comes only for text we did not see any issue while drawing the images. As we cache both the fonts and images upfront during the initialization though we are seeing the issue with text(fonts).
Solved! Go to Solution.
2023-09-26 12:50 AM
To address the issue of garbled text in your TouchGFX application:
2023-06-13 5:57 AM
Hello @Community member,
Could you provide a picture/screenshot of this problem please ?
Thanks,
/Yoann
2023-06-21 3:21 AM
Hi, we have found the root cause of this issue. It was regarding the common memory operation used by both firmware upgrade process and Touchgfx process. As we are using unmapped fonts storing it in external memory the data reader used by touchgfx task perform memory read operation to get font data at the same time firmware upgrade task use memory write operation. To resolved this issue we implement Mutex to avoid multiple task using same utility.
2023-06-29 3:55 AM
Hi Ashah
Nice. Do you think we should add something in the documentation?
Regs
2023-09-26 12:50 AM
To address the issue of garbled text in your TouchGFX application:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.