2020-02-05 9:29 PM
Done
Post Generate
touchgfx update_project --project-file=../EWARM/application.ewp && touchgfx update_project && touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
No value provided for required options '--project-file'
Failed
Failed
Running the Application.sln gives build errors with
Severity Code Description Project File Line Suppression State
Error LNK2019 unresolved external symbol "public: __thiscall HallwayScreenViewBase::HallwayScreenViewBase(void)" (??0HallwayScreenViewBase@@QAE@XZ) referenced in function "public: __thiscall HallwayScreenView::HallwayScreenView(void)" (??0HallwayScreenView@@QAE@XZ) Application C:\TouchGFXProjects\MyApplication_3\Projects\TouchGFX\simulator\msvs\hallwayScreenView.obj 1
and
Severity Code Description Project File Line Suppression State
Error LNK2019 unresolved external symbol "public: virtual void __thiscall HallwayScreenViewBase::setupScreen(void)" (?setupScreen@HallwayScreenViewBase@@UAEXXZ) referenced in function "public: virtual void __thiscall HallwayScreenView::setupScreen(void)" (?setupScreen@HallwayScreenView@@UAEXXZ) Application C:\TouchGFXProjects\MyApplication_3\Projects\TouchGFX\simulator\msvs\hallwayScreenView.obj 1
2020-02-17 2:30 AM
Hi,
The resulting build errors are because the post-generate fails (it cannot update your project with HallWayScreenView.cpp.
I'm not sure what happened to your post generate command, but open your .touchgfx file and remove this part
&& touchgfx update_project &&It should work then, updating EWARM and MSVS projects.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.