2022-09-15 10:12 AM
My project uses LTDC as application tick source and two frame buffers. I am trying to understand:
1. What the current frame rate (I understand this is same as vSync frequency) is. I know it can be measured by monitoring vSyncFreq GPIO. But I want to see where it is in code.
2.What are the steps to change frame rate? I would like to see it in code please.
If frame rate is change is achieved by changing the pixel clock, what is the relation between two.
I appreciate your help.
Solved! Go to Solution.
2022-09-15 10:20 PM
2022-09-15 10:22 AM
Your reply is in your question. Framerate based on LTDC is based on DCLK = dot clock. LTDC clock in MX clock config.
Calculating frame rate then is based on DCLK / ( HOR x VERT ) ... sum of porch and sync include.
Example for 800x480 LCD and DCLK 33MHz
FR = 33M / ( 840x520 ) = 75,55 Hz
This is true only for LCDs in video mode RGB, displays with own memory or other interfaces (SPI ...) works other way.
2022-09-15 10:41 AM
"LTDC clock in MX clock config"
Is it possible to see this in generated code?
"sum of porch and sync include"
is it both front and back porch? i.e. front porch + back porch + sync?
2022-09-15 10:20 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.