2022-07-08 10:44 PM
Hi ,
I am trying to implement a project with STM32H753i evaluation board with LCD TFT display. In that I want to implement GUI interface using STemWin application. I have referred the example 'Hello world' project but I am not able get STemWin graphics option using STM32CubeMX and STM32CubeIDE in my standalone project while creating. Is there any way to get STemWin application in the STMCubeMX for STM32H753i evaluation board please give any suggestion.
I have also tried with older version of cubeMX(4.26) but could not configure.
Software used:
STMCubeMx V6.1.2
STMCUbeIDE V1.10.0
2022-07-08 11:17 PM
Getting started with STemWin Library
add it manualy or use TouchGFX ...
2022-07-08 11:49 PM
Thank you for the reply.
I have tried with GFX but for STM32H753I board selection is not there and because of that it is getting link errors. STM32H743I is the only selection option for H7 series. I will follow the document and try once.
2022-07-09 12:16 AM
?? Open IDE create new project choice board ... in MX plugin ioc edit window click software pack and add TouchGFX ...
And yes prepared examples is only for some chips, but usable is all.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.