cancel
Showing results for 
Search instead for 
Did you mean: 

How to get an external HDMI display working with STM32F769I-DISCO + B-LCDAD-HDMI using touchGFX and STMCUBEIDE

TGood.1
Associate II

Hi, I have so far successfully used TouchGFX to create GUI that ineracts with a button press (Later this will be ported to interact with CANBUS)….I digress.

Now I want to add a bigger 5inch screen (Still waiting on DSI Displays to turn up) So using the B-LCDAD-HDMI interface to take the DSI signals to drive a HDMI display - Thought this may have been easier than it looked. Anyway I read somewhere else on here about the need to add #define USE_LCD_HDMI - However where should this be added? and what are you defining? normally there is a value!?

Setup is STM32F769I-DISCO + B-LCDAD-HDMI using touchGFX and STMCUBEIDE

So at the moment all I get is a blank screen … Screen works (already checked that).

Any help appreciated?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.