STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! I want to create a parameter setting screen

Thank you for helping.environment:STM32F769I-DISCOTouchGFX4.12.3STM32CubeIDE1.3.0I want to create a screen for setting parameters such as IP address.(1)Is there a text box to enter in the UI? If not, how can this be achieved?(2) How can you display t...

Ebun.1 by Senior
  • 1882 Views
  • 7 replies
  • 0 kudos

Question upon STM32F103, DCMI and PAL driver

Hello everyone~ Hope you guys are doing well.I am recently working on OV2640 with STM32F103. As far as I discovered, most of the source code I found on the internet are OV2640 with F4 or F7 series, which are compatible with DCMI. And obviously F103 d...

WAi.11 by Associate II
  • 2665 Views
  • 4 replies
  • 0 kudos

Numeric keyboard and alphabet keyboard together?

Hello every one. In most project it's need to have two kind of keyboard for input number and also input alphabet characters. In the keyboard example that comes with touchgfx it's possible to input both alphabet and number. But if for input just numbe...

S.Mirza by Associate II
  • 1172 Views
  • 1 replies
  • 0 kudos

Hello I set up TouchGFX and when I want to simulate, I get an error like the following. It doesn't work on Code Generator and Run Target.

Run Simulator  Copy Framework    Copying TouchGFX framework version 4.13.0 to C:\TouchGFXProjects\MyApplication\Middlewares\ST\touchgfx    Done  Generate    Wrote config/gcc/app.mk    Wrote config/msvs/Application.props    Wrote generated/gui_generat...

I am getting HardFault error while using GUI_PNG_DrawEx function of stEmWin library. What is wrong with my project?

I have achieved to draw bmp, gif and jpg images with related DrawEx functions of stEmWin library. The library version of stEmWin is 544. In order to try png images, I downloaded png library from segger's web site. I imported the source files of the p...

CSeng.1 by Associate
  • 1370 Views
  • 1 replies
  • 0 kudos

How to get an external HDMI display working with STM32F769I-DISCO + B-LCDAD-HDMI using touchGFX and STMCUBEIDE

Hi, I have so far successfully used TouchGFX to create GUI that ineracts with a button press (Later this will be ported to interact with CANBUS)….I digress.Now I want to add a bigger 5inch screen (Still waiting on DSI Displays to turn up) So using th...

TGood.1 by Associate II
  • 899 Views
  • 0 replies
  • 0 kudos

Shift Graph

Hi ST,I have a problem when draw graph. when i set size 400 and shift graph, its ok. But if set size 800, it has issue as image. Code shift graph:graphLine.setBuffer(graphBuffer, NUMBER_OF_POINTS);//shift datafor (int i = 1; i < NUMBER_OF_POINTS; i++...

NHo.1 by Associate III
  • 2422 Views
  • 4 replies
  • 0 kudos

Resolved! I want to change main.c to main.cpp

environment:STM32CubeIDE Ver 1.3.0STM32CubeMX Ver 5.5.0TouchGFX Ver 4.13.0Load the project created with TouchGFX in the IDE.How can I change main.c to main.cpp and let the IDE understand?Thank you.

Ebun.1 by Senior
  • 2236 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.