2022-10-02 11:16 AM
I'm making a custom keyboard and want to add some extra functionality. I need to be able to edit the texts (i.e. by marking the place of the text and moving the entire text to the right when writing). Maybe someone has done something similar and can help?
2022-10-02 11:50 PM
Hello @heyo ,
I don't know about the extra functionalities you are asking for, but if you want a ready-to-use keyboard, you can download the one we made here.
Hope that this helps,
/Yoann
2022-10-03 12:25 AM
@Yoann KLEIN I want to do that i can edit text, for example touch anywhere in text string and start write from that point. But then I change buffer position and start to write all letters after cursor dissapear . Im using setBufferPosition function.
2022-10-03 5:23 AM
Hello @heyo ,
I did a example for you, I will join the project for you to this post.
To explain quickly what I did :
void Keyboard::textAreaClickHandler(const TextAreaWithOneWildcard& b, const ClickEvent& event)
{
int x = event.getX();
int y = event.getY();
}void Keyboard::textAreaClickHandler(const TextAreaWithOneWildcard& b, const ClickEvent& event)
{
int x = event.getX();
int y = event.getY();
touchgfx::Unicode::snprintf(textArea1Buffer1, TEXTAREA1BUFFER2_SIZE, "%d", x);
touchgfx::Unicode::snprintf(textArea1Buffer2, TEXTAREA1BUFFER2_SIZE, "%d", y);
textArea1.invalidate();
}void Keyboard::textAreaClickHandler(const TextAreaWithOneWildcard& b, const ClickEvent& event)
{
int x = event.getX();
int y = event.getY();
touchgfx::Unicode::snprintf(textArea1Buffer1, TEXTAREA1BUFFER2_SIZE, "%d", x);
touchgfx::Unicode::snprintf(textArea1Buffer2, TEXTAREA1BUFFER2_SIZE, "%d", y);
textArea1.invalidate();
positionText = x/10;
}Of course, this is just an example to show you how to do it. It's something not robust at all, because that will only work if all the glyphs of your font have approximately the same dimensions, which is often not the case.
If you want something better, but without the click feature, you can take a look at this post.
It describes how to implement a cursor in a TextArea and move it manually by clicks on a button on the display.
Hope that I helped you starting your development,
/Yoann
2022-10-03 5:28 AM
2022-10-03 5:55 AM
Thank you @Yoann KLEIN . Maybe you don't understand me. I realized cursor before and I can move cursor whatever I want, problem is that I can't edit text. For better understanding I try to explain you more. So I'm trying to make that with keyboard can be edit texts because now then I change cursor position for example in a middle of text: and start writing from that point, letters after cursor gone(I write "e" letter):
So I want that text looks like this then I write "e".
I think that buffer needs to be shifted from that point where I clicked and "e" inserted in buffer, but I try a lot of variants and nothing works yet. Maybe then I set buffer position with "setBufferPos" function all other letters deletes from buffer. Maybe you have any suggestions?
2022-10-04 12:37 AM
Hello,
I succeeded doing that easily by :
#include <string>
using namespace std;string str_buffer = buffer;
string str_value(1, value);str_buffer.insert(positionText,str_value);strcpy(buffer, str_buffer.c_str());Unicode::strncpy(keyboardTextAreaBuffer, buffer, KEYBOARDTEXTAREA_SIZE); //assign the string to the Text
keyboardTextArea.resizeToCurrentText();
keyboardTextArea.invalidate();Finally, my whole function becomes :
void Keyboard::writeButtonCharacter(char value){
// value-> corresponds to the character associated with the button that was clicked
positionText++;
if (positionText<=60){ // string length limit
string str_buffer = buffer;
string str_value(1, value);
str_buffer.insert(positionText,str_value);
strcpy(buffer, str_buffer.c_str());
Unicode::strncpy(keyboardTextAreaBuffer, buffer, KEYBOARDTEXTAREA_SIZE); //assign the string to the Text
keyboardTextArea.resizeToCurrentText();
keyboardTextArea.invalidate();
}
}That should make it, let me know if you have other issues.
/Yoann
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.