2022-11-03 10:26 PM
2022-11-03 11:42 PM
Hi,
TouchGFX follows the Model-View-Presenter architecture. You can communicate between the hardware and the gui through the Model. I suggest to read this "Backend Communication" article on the online documentation which explains this process and how to communicate with the hardware.
I can also recommend this video from Gustavo on the ST youtube channel where Gustavo explains how to communicate between a button and the UI or how to turn on and off a LED through the UI with TouchGFX.
2022-11-04 12:01 AM
thanks, one more things i want to know is that how i can receive 10 urat data ,
can i use a buffer to store these data and after display it . any other methods
more info:
actually i worked on a project with UI setup. use two stm32 borads, one for data reading(adc) and pass data over urat to second one (stm32+display_touch gfx), so i wanted to start the reading when i do something in touch gfx gui like button click, slider etc. after reading first one transfer data to second one and the informations are displayed in ui view like a table with column and rows.
2022-11-04 12:03 AM
so if i recieve 10 data it will displayed in 10 different location
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.