2016-11-22 1:10 AM
i'm trying to display a visual output by using
TVP5150AM1 Decoder and STM32F429II MCU.
Is it possible to get CCIR656(TVP5150AM1) format with DCMI(STM32F429II) input? (On manual it's possible)
If it is, How do I configure the settings of
DCMI_ESCR register and DCMI_ESUR register?
Visual format is NTSC 720*480, CCIR656(Embedded data synchronization mode).
If there are any reference manual or data, please inform me.
#ccir656 #dcmi #stm32f4292016-11-22 2:39 AM
Hello,
'TVP5150' Decoder is working in mode ITU656 and it's possible to get CCIR656 fromat with DCMI input.As described in the RM0090, page 463: DCMI Interface is configured in Snapshot mode and to use Embedded data synchronization mod: Mode 1 An alternative coding is the camera mode 1. This mode is ITU656 compatible.Make a search in the Forum with keywords: TVP5150, ITU656, DCMI_ESCR, DCMI_ESUR, DCMI..., maybe you will find several threads on the topic that helps you on the configuration settings.
Regards2016-11-22 11:42 PM
Many thanks
Your answer helps me a lot.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.