2016-11-17 11:43 AM
Hello all, I am trying to configure my STM32F407VGT in CubeMX and am coming across an issue with the DCMI and FSMC. I am interfacing an OVM7690 camera chip to the microcontroller via DCMI. The OVM7690 requires an 8-bit external synchronous connection which configures just fine in CubeMX.
However, when I go to configure the FSMC, it doesn't allow me to select a Muxed PSRAM configuration because of the DCMI configuration, which is what I also need to interface to the micro. I assume it is because both of those peripherals can't be used at the same time but I don't see anything in the data sheet that says why that is. Does anyone know the reason? Is the best solution to upgrade to a 144 pin version?Thank you in advance. #stm32f4-fsmc-dcmi-psram2016-11-18 12:07 AM
Hello,
Looking at the STM32F407xx shows the PB7 pin used as alternate function DCMI_VSYNC and FSMC_NL (for LQFP100 package). Refer to the page 58: Table 7. STM32F40xxx pin and ball definitions.Maybe you can use the UFBGA176 package, which allow using PI5 as DCMI_VSYNC and PB7 as FSMC_NL .RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.