2021-06-29 3:59 AM
Suppose I create a container called 'containers' which has further other containers called container1, container2 and container3.
Now how can I iterate the inside containers from the outer container? Is it even possible in TouchGFX?
My intention is to control whether to set particular container visible or invisible.
2021-07-08 1:49 AM
Hi BParh.1,
This one is a bit tricky but here is a code example :
void Screen1View::containerIterate()
{
Drawable* d = topContainer.getFirstChild(); // get the first child inside your top container. This child is also a container.
// Important to notice that d is a Drawable so you need to cast it to the widget type you need. See below with the Box widget
while (d) // loop through the Drawables
{
// Here we just have some Box inside a (child)container that we set in Black as an example. But you can have other widgets inside your (child)container
Box* boxChild;
boxChild = (Box*)d->getFirstChild();
boxChild->setColor(Color::getColorFromRGB(0x00, 0x00, 0x00));
d = d->getNextSibling(); // This is how you can get the next child inside the top container
}
topContainer.invalidate(); // Do not forget to invalidate
}For your specific request, that is to control if a container is visible or not, here is the code sample :
void Screen1View::containerIterate()
{
Drawable* d = topContainer.getFirstChild();
while (d)
{
d->setVisible(!d->isVisible());
d = d->getNextSibling();
}
topContainer.invalidate();
}Hope it helps,
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.