2018-12-19 11:36 PM
When I tried USB Host standalone examples software goes to SPDIF_RX_IRQHandler. I think the problem is about queue from ISR.
2018-12-20 12:43 AM
Hi,
What exactly is the problem you're having and what are you trying to accomplish?
Thanks!
Best regards,
Martin
2018-12-20 12:52 AM
thanks for reply
I tried a lot of examples. Firstly I tried USB host MSC_Standalone example. When I tried integrate this example to TouchGFX any project, while USB is attached screen is frozen. In debugging stops on SPDIF_RX_IRQHandler
Firstly I create task as following
xTaskCreate(GUITask, (TASKCREATE_NAME_TYPE)"GUITask", configGUI_TASK_STK_SIZE, NULL, configGUI_TASK_PRIORITY, NULL);
xTaskCreate(MainTask, (TASKCREATE_NAME_TYPE)"MainTask", 1250, NULL, configGUI_TASK_PRIORITY+1, NULL);
static void MainTask(void* params){
USB_Init();
while(1){
vTaskDelay(50);
mainwhileusb();
}
}
void USB_Kur(void){
USBH_Init(&hUSBHost, USBH_UserProcess, 0);
USBH_RegisterClass(&hUSBHost, USBH_MSC_CLASS);
USBH_Start(&hUSBHost);
}
void mainwhileusb(void){
USBH_Process(&hUSBHost);
}
2018-12-20 1:17 AM
What is your application doing? Are you in a hardfault or is the GUI task blocked?
2018-12-20 1:24 AM
Any hardfault is seen. But now in SPDIF_RX_IRQHandler
2018-12-20 1:27 AM
I am using Keil and working with STM32f746 DISCO
2018-12-20 2:34 AM
Maybe you could cross reference the configuration of the examples you've been running vs the TouchGFX application? Are you sure your interrupt configuration is correct? E.g. Why are you hitting the SPDIF_RX_IRQHandler?
2018-12-20 3:06 AM
USB_Init is from working example (not using TouchGFX) so I dont think wrong interrupt configurations. But I dont know interrupt configurations for freertos and freertosconfig.h. No example on internet for TouchGFX including USB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.