2019-06-29 6:57 AM
Hi,
I want to try to use 8BPP in one of the project I'm working on.
I set the LTDC to work in 8BPP and I tried to define a designer project that is configure with 8bpp.
When I try to change the config I get error messages that I can not use this format
2019-06-30 1:29 PM
Hi Eyal,
ARGB2222 (8-bit) is supported in TouchGFX 4.11+. Even though the release is completed and we have the binary, it's not officially released because of internal release dependencies. 4.12 will be out as soon as CubeMX 4.4.0 is released.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.