2022-04-09 11:48 AM
I want to drive 1.44 TFT with stm32f303 but flash is overflow. Can you help me? How about optimization touchgfx? In addition i dont use external flash.
2022-04-09 11:17 PM
Memory ranges from 32 to 512 Kbytes and packages from 32 to 144 pins ???
2022-04-10 12:18 AM
Memory is 256k but i can use 110k for touchgfx. Package from 48 pins. (stm32f303cct6)
2022-04-10 4:00 AM
This is edge, images set to L8 and optimization levels set to size
2022-04-10 4:40 AM
Even if I only describe it, it takes 70k flash. Only one empty box is defined. Optimization level is size
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.