2019-12-11 1:41 AM
2019-12-11 2:43 AM
I need way more information than that :) Version? What've you tried? Share your project?
Thanks
2019-12-12 7:08 AM
2019-12-12 7:25 AM
2020-01-06 11:35 PM
Hi,
do you have an idea for this problem?
Regards,
2020-01-06 11:51 PM
Hi Luca,
4.13.0 will be out this week so let's see if that solves things for you. I'm pretty sure we've fixed an issue similar to what you're seeing here.
/Martin
2020-01-08 2:20 AM
Hi, I have simillar issue with Cubemx 5.5.0 and TouchGFX 4.13.0
error msg : "Object reference not set to an instance of an object."
2020-01-08 4:07 AM
Are you trying to open up a possibly broken project in 4.13.0 ? Please show me a log for 4.13.0.
2020-01-22 4:16 PM
Is there a solution for this? I am having the same problem in my project. I was trying to upgrade my project from 4.12.3 to 4.13 and ran into this error. I can message the zip of my project if necessary.
2020-01-22 11:31 PM
I still have the same problem with 4.13
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.