2021-10-13 4:26 AM
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project --project-file=../nfc_4.ioc --platform=m4
.project files generated inside project folder
This is STM32CubeIDE project updater: Working on ../STM32CubeIDE/.project
Project file: ../STM32CubeIDE/.cproject
Done
Compile
make -f ../gcc/Makefile -j10
Reading TouchGFX/application.config
Generating TouchGFX/generated/texts/src/Texts.cpp
Generating TouchGFX/generated/texts/src/LanguageGb.cpp
Compiling TouchGFX/gui/src/common/CustomKeyboard.cpp
Compiling TouchGFX/generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/screen8_screen/Screen8ViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/screen6_screen/Screen6ViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/screen4_screen/Screen4ViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/screenkeyboard3_screen/Screenkeyboard3ViewBase.cpp
TouchGFX/gui/src/common/CustomKeyboard.cpp: In constructor 'CustomKeyboard::CustomKeyboard()':
TouchGFX/gui/src/common/CustomKeyboard.cpp:22:5: error: 'memset' was not declared in this scope
memset(buffer, 0, sizeof(buffer));
^~~~~~
TouchGFX/gui/src/common/CustomKeyboard.cpp:29:30: error: 'Color' has not been declared
modeBtnTextArea.setColor(Color::getColorFrom24BitRGB(0xFF, 0xFF, 0xFF));
^~~~~
TouchGFX/gui/src/common/CustomKeyboard.cpp: In member function 'touchgfx::Unicode::UnicodeChar* CustomKeyboard::getBuffer1()':
TouchGFX/gui/src/common/CustomKeyboard.cpp:131:21: error: 'class touchgfx::Keyboard' has no member named 'getBuffer1'; did you mean 'getBuffer'?
return keyboard.getBuffer1();
^~~~~~~~~~
getBuffer
TouchGFX/gui/src/common/CustomKeyboard.cpp: In member function 'touchgfx::Unicode::UnicodeChar* CustomKeyboard::getBuffer2()':
TouchGFX/gui/src/common/CustomKeyboard.cpp:136:21: error: 'class touchgfx::Keyboard' has no member named 'getBuffer2'; did you mean 'getBuffer'?
return keyboard.getBuffer2();
^~~~~~~~~~
getBuffer
make[2]: *** [TouchGFX/build/STM32F469-DISCO/TouchGFX/gui/src/common/CustomKeyboard.o] Error 1
gcc/Makefile:329: recipe for target 'TouchGFX/build/STM32F469-DISCO/TouchGFX/gui/src/common/CustomKeyboard.o' failed
make[2]: *** Waiting for unfinished jobs....
Compiling TouchGFX/generated/gui_generated/src/screen3_screen/Screen3ViewBase.cpp
TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.cpp: In member function 'void Screen2ViewBase::buttonCallbackHandler(const touchgfx::AbstractButton&)':
TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.cpp:111:9: error: 'few' was not declared in this scope
few seconds
^~~
TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.cpp:111:9: note: suggested alternative: 'View'
few seconds
^~~
View
make[2]: *** [TouchGFX/build/STM32F469-DISCO/TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.o] Error 1
gcc/Makefile:329: recipe for target 'TouchGFX/build/STM32F469-DISCO/TouchGFX/generated/gui_generated/src/screen2_screen/Screen2ViewBase.o' failed
make[1]: *** [generate_assets] Error 2
gcc/Makefile:296: recipe for target 'generate_assets' failed
make: *** [all] Error 2
../gcc/Makefile:47: recipe for target 'all' failed
Failed
Failed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.