2019-05-26 11:06 AM
here is my code
void LCD_Enable()
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_14,1);
HAL_Delay(1);
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_14,0);
HAL_Delay(1);
}
void LCD_Send4Bit(unsigned char Data)
{
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_8,Data&0x01);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_9,(Data>>1)&0x01);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_10,(Data>>2)&0x01);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_11,(Data>>3)&0x01);
}
void LCD_SendCommand(unsigned char command)
{
LCD_Send4Bit(command >>4);/* Gui 4 bit cao */
LCD_Enable();
LCD_Send4Bit(command); /* Gui 4 bit thap*/
LCD_Enable();
}
void LCD_Clear()
{
LCD_SendCommand(0x01);
HAL_Delay(1000);
}
/* USER CODE END 0 */
void LCD_Init()
{
LCD_Send4Bit(0x00);
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_12,0);
LCD_Send4Bit(0x03);
LCD_Enable();
LCD_Enable();
LCD_Enable();
LCD_Send4Bit(0x02);
LCD_Enable();
//LCD_SendCommand(0x33);
//HAL_Delay(100);
//LCD_SendCommand(0x32);
//HAL_Delay(500);
LCD_SendCommand(0x28); // giao thuc 4 bit, hien thi 2 hang, ki tu 5x8
//HAL_Delay(500);
//LCD_SendCommand(0x01);
//HAL_Delay(500);
//LCD_SendCommand(0x06); // cho phep hien thi man hinh
//HAL_Delay(500);
LCD_SendCommand(0x0C); // tang ID, khong dich khung hinh
//HAL_Delay(500);
LCD_SendCommand(0x06); // xoa toan bo khung hinh
LCD_SendCommand(0X01);
//HAL_Delay(500);
}
void LCD_PutChar(unsigned char Data)
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_12,1);
LCD_SendCommand(Data);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,0);
}
void LCD_Puts(char *s)
{
//LCD_Gotoxy(x,y);
while (*s){
LCD_PutChar(*s);
s++;
}
}
void LCD_Gotoxy(unsigned char x, unsigned char y)
{
unsigned char address;
if(!y)address=(0x80+x);
else address=(0xC0+x);
LCD_SendCommand(address);
}
/**
* @brief The application entry point.
*
* @retval None
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
LCD_Init();
//LCD_Gotoxy(1,1);
// LCD_Puts("NEPAL");
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
LCD_Gotoxy(1,1);
LCD_Puts("NEPAL");
HAL_Delay(1500);
LCD_Clear();
}
/* USER CODE END 3 */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.