2023-10-10 6:54 AM
Hi.
I wish to modify some of the header files in TouchGFX itself.
Concretely: I want to add both data members and virtual methods to:
- touchgfx/containers/Container.hpp
- mvp/Presenter.hpp
Possible? No... The windows simulator crashes.
Why? Most likely because one links to msvs/libtouchgfx_v143.lib which contains source files that absolutely expects those header files to not be edited.
Then I try to compile all the source files instead of linking to the prebuilt one.
Works? No… Some of the secret stuff cannot be found as source code. That’s fair. It’s a commercial product.
But then what?
The core files should be hackable enough that developers can build their own frameworks around them.
How about splitting the libraries into two parts: One for the files that cannot be shared and the other for files that can.
Cheers
2023-11-02 5:20 AM
Hello @ReneJensen ,
Thank you for your suggestion. We will consider it, but can I ask what are the changes that you would like to implement?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.