2023-02-16 8:17 AM
Hello,
TouchGfx v4.17.0
CubeIDE v1.11.2
I am using the .ioc UI to add an analogue pin for use with GUI, but when I save and generate code, it removes several TouchGfx files making code uncompilable, am I missing something in TouchGfx set up from CubeIDE?
TouchGfx itself generates code fine into CubeIDE and the deployment to board is also fine, I suspect there is just some buried option I am missing hopefully. Re-generating code from TouchGfx Designer doesn't repair missing files
Thanks
2023-02-22 1:00 AM
I'm not too sure.. I've managed to narrow down the issue to just 1 error today, 'STM32DMA.hpp: No such file or directory' even though the header file is still available. My other files are generally untouched when generating
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.