2025-04-09 12:00 AM
It turns out the GDB shipped with TouchGFX 4.25.00 has an issue where it can't set the breakpoint in VSCode when the software is running.
The only workaround is to set the breakpoints before launching the debug.
The issue is reported it https://github.com/microsoft/vscode-cpptools/issues/13191#issuecomment-2787932838
To fix the issue you can use the GDB shipped with the latest version of MYSYS2 https://packages.msys2.org/packages/mingw-w64-x86_64-gdb
You just run on the terminal pacman -S mingw-w64-x86_64-gdb
In the launch.json you set "miDebuggerPath": "C:/msys64/mingw64/bin/gdb.exe", (or the location where it has been installed) and in the task.json in "env": {"PATH": "C:/msys64/mingw64/bin;"}
Solved! Go to Solution.
2025-11-28 12:28 AM
The GDB shipped with TouchGFX has a bug that won't let you set a breakpoint while debugging in VSCode
The workaround (not a fix) is to install MYSYS2 in your system. After that, you can run the MYSYS2 cmd console and install gdb with:
pacman -S mingw-w64-x86_64-gdbAt this point, in the launch.json, you can use "miDebuggerPath": "C:/msys64/mingw64/bin/gdb.exe"
2025-04-11 12:53 AM
Hello @nico23,
Thanks for your workaround, I will talk to the team about that.
You use VScode to debug on target ?
BR,
2025-04-11 12:59 AM
Hi Louis,
No, to debug the target I'm using CubeIDE.
I'm using VSCode to debug the Simlutor on my machine as using Visual Studio is not suitable for me
2025-11-28 12:28 AM
The GDB shipped with TouchGFX has a bug that won't let you set a breakpoint while debugging in VSCode
The workaround (not a fix) is to install MYSYS2 in your system. After that, you can run the MYSYS2 cmd console and install gdb with:
pacman -S mingw-w64-x86_64-gdbAt this point, in the launch.json, you can use "miDebuggerPath": "C:/msys64/mingw64/bin/gdb.exe"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.