2018-06-14 12:52 AM
Hi,
When I write to the FCR register (via HAL_LCD_Init) , the FCRSF is not being set afterwards and so the LCD_WaitForSynchro is failing.
/* Loop until FCRSF flag is set */
while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_FCRSF) == RESET){if((HAL_GetTick() - tickstart ) > LCD_TIMEOUT_VALUE){hlcd->ErrorCode = HAL_LCD_ERROR_FCRSF;return HAL_TIMEOUT;}}This is code generated for the STM32L152c discovery board by STMCube32. I assume this is to do with domain clock sync, but not sure what the fault is.
Many Thanks
#fcrst #lcd #fcr2018-07-16 6:20 AM
I have figured this out. The RTC Clock Select was not being set. Once I added
RCC->CSR |= RCC_CSR_RTCSEL_LSE;
to select the Low-Speed External clock, it worked and the FCRSF flag is being set. The default value is Zerto is 'No Clock' and as the LCD shares the RTC clock signal this needs to be set before it can work.
Hope this helps
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.