2020-03-18 9:32 AM
When I add my second FlexButton to any screen, and click "Can trigger another interaction", for that FlexButton I get the error in the "Run Simulator" build of the project.
error: 'FlexButton' is not a member of 'touchgfx'
By unchecking, the "Can trigger another interaction", the problem immediately goes away.
Noted this case immediately, when I was testing with custom containers, and had 3 containers on a screen.
The custom container, had a flex button, to Fade something in the custom container.
Using
TouchGFX, 4.12.3
2020-03-31 8:03 AM
Hi,
TouchGFX 4.13.0 is out. Tried it there?
/Martin
2020-03-31 9:01 AM
Still the same behavior in 4.13
When I have the Flex button in a container, and I add the fade out interaction on this button, then when the interaction is complete, I do the fade in interaction.
I get the following on the gcc compile.
In file included from gui/include/gui/containers/CustomContainerButtons.hpp:4:0,
from generated/gui_generated/include/gui_generated/mainscreen_screen/MainScreenViewBase.hpp:13,
from gui/include/gui/mainscreen_screen/MainScreenView.hpp:4,
from gui/src/mainscreen_screen/MainScreenView.cpp:1:
generated/gui_generated/include/gui_generated/containers/CustomContainerButtonsBase.hpp:88:93: error: 'FlexButton' is not a member of 'touchgfx'
touchgfx::Callback < CustomContainerButtonsBase, const touchgfx::FadeAnimator<touchgfx::FlexButton>& > interaction23EndedCallback;
^~~~~~~~~~
generated/gui_generated/include/gui_generated/containers/CustomContainerButtonsBase.hpp:88:93: note: suggested alternative: 'Button'
touchgfx::Callback < CustomContainerButtonsBase, const touchgfx::FadeAnimator<touchgfx::FlexButton>& > interaction23EndedCallback;
^~~~~~~~~~
Button
VS2017
On this line of code
touchgfx::Callback < CustomContainerButtonsBase, const touchgfx::FadeAnimator<touchgfx::FlexButton>& > interaction23EndedCallback;
This error is generated
1>c:\touchgfxprojects\customcontainertest_4_13\generated\gui_generated\include\gui_generated\containers\customcontainerbuttonsbase.hpp(88): error C2039: 'FlexButton': is not a member of 'touchgfx' (compiling source file ..\..\simulator\main.cpp)
1>c:\touchgfxprojects\customcontainertest_4_13\touchgfx\framework\include\touchgfx\containers\buttons\buttons.hpp(34): note: see declaration of 'touchgfx' (compiling source file ..\..\simulator\main.cpp)
1>c:\touchgfxprojects\customcontainertest_4_13\generated\gui_generated\include\gui_generated\containers\customcontainerbuttonsbase.hpp(88): error C2065: 'FlexButton': undeclared identifier (compiling source file ..\..\simulator\main.cpp)
1>c:\touchgfxprojects\customcontainertest_4_13\generated\gui_generated\include\gui_generated\containers\customcontainerbuttonsbase.hpp(88): error C2923: 'touchgfx::FadeAnimator': 'FlexButton' is not a valid template type argument for parameter 'T' (compiling source file ..\..\simulator\main.cpp)
1>c:\touchgfxprojects\customcontainertest_4_13\generated\gui_generated\include\gui_generated\containers\customcontainerbuttonsbase.hpp(88): error C2955: 'touchgfx::FadeAnimator': use of class template requires template argument list (compiling source file ..\..\simulator\main.cpp)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.