2022-01-20 8:44 AM
When i generate code through the TouchGFX Designer it always generates the code to run mainly in the cm7 core, but i want ot use this core to do some heavy computation. Any help? Thanks
2022-01-26 7:44 AM
Defining if a thing is difficult is as well difficult as it depends on the person. You do have the documentation and videos on how to set TouchGFX and the TouchGFX Generator for single core MCUs as shared. The dual core just implies a more complex structure and a more complex STM32CubeMX file :downcast_face_with_sweat:. This is the time consuming part in my opinion, because otherwise most of the user code is already set in the TBS for the STM32H747dk so it can be copy pasted or used as source of inspiration/base for other files to set. I believe theere will be other settings to do with the toolchain you use.
It is an interesting thing to do, I don't have the time to do it in the coming days but it is something I can try to do if you have 2 weeks.
/Romain
2022-01-26 8:55 AM
Sure, please do. It would be a great help.
Thank you Romain, looking forward to hearing from you back.
2022-02-15 1:49 PM
Hey, just wanted to check up if you managed to achieve this. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.