2019-05-28 1:42 PM
I try to add a very simple screen to my project. It always crashed when I try to add a box as background. It ends up with the infinite loop in startup assembly file.
Here is what I found so far:
I am using f7 and has set clock and SDRAM to maximum speed. Does anyone has similar issue? Is there any settings to improve this issue? Thanks in advance.
Solved! Go to Solution.
2019-06-03 2:21 AM
Hi @zzzzz,
Is this a custom board? Have you checked your LTDC and DMA registers for errors?
A few things to try just to see if there are any improvements:
Let me know
/Martin
2019-06-03 2:21 AM
Hi @zzzzz,
Is this a custom board? Have you checked your LTDC and DMA registers for errors?
A few things to try just to see if there are any improvements:
Let me know
/Martin
2019-06-06 2:08 PM
Thanks for your reply!
Yes, it is a custom board and it works well with STemWin before.
No error flag is set in LTDC or DMA2D registers.
I have tried hal.lockDMAToFrontPorch(true). It is not solve the issue.
Could you explain how to use NoDMA class? Does that mean I need modify STM32F7DMA.cpp?
Thanks.
2019-06-06 11:29 PM
Hi @zzzzz,
You simply declare a different DMA class than the one you're using. Let me exemplify:
//BoardConfiguration.cpp
#include <touchgfx/hal/NoDMA.hpp>
//STM32F7DMA dma;
NoDMA dma;
STM32F7TouchController tc;
STM32F7Instrumentation mcuInstr;
2019-07-11 10:57 PM
@Martin KJELDSEN
Sorry for using this thread.
I have a similar issue using the STM32F469I-DISCO and I have been looking into your suggestions
and the NoDMA solves my issue. The question now is what it means. What am I going
the chase to resolve the problem to reenable the DMA?
I’m using STM32CubeIDE 1.01.
Best regards
Thomas
2019-07-11 11:27 PM
Hi @TDahl,
The F469I-DISCO should not have this issue. Locking the DMA to the front porch is a trick you can use if you've got issues with LTDC and DMA accessing the memory at the same time. In this case you can either slow down the application somewhat (lowering pixel clock, increasing porch areas within spec, locking DMA to front porch).
CubeIDE/CubeMX will not necessarily create the best configuration for TouchGFX. Try creating an application from our TouchGFX designer using the 469-DISCO applicaiton template and compare the configurations, maybe. It for sure works.
/Martin
2019-07-11 11:44 PM
Thanks @Martin KJELDSEN
I will try that.
Thomas
2019-07-12 1:44 AM
For reference I seem to have solved the problem by halving the LCD-TFT clock because of double buffering. Thanks again @Martin KJELDSEN
/Thomas
2019-07-12 2:53 AM
Awesome, Thomas!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.