2023-02-16 5:57 AM
2023-02-17 5:07 AM
Could you try to download that zip folder.
Then copy it inside the C:\Users\USERNAME\AppData\Roaming\TouchGFX-4.21.1\Downloads\STM32H7B3I-DK\3.0.12 folder and replace its extension with ".tpa".
Then open TouchGFXDesigner again and let me know if it works.
/Yoann
2023-02-17 12:48 AM
Hello @stefanHriellström,
I just succeeded to download it on my computer, with the same version.
Did you check your internet connection ? If you don't have internet, or if TouchGFXDesigner cannot access to the server to download the TouchGFX Board setups, a red warning triangle should appear on the top left corner of the home screen.
/Yoann
2023-02-17 12:49 AM
Hello @stefanHriellström and welcome to STCommunity :) ,
I have checked from my side and I cannot reproduce this issue.
I recommend you to follow properly the steps as described in this MOOC.
Also, I advise you to take a look at this article.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-17 1:01 AM
Very strange!
Other tested board setups was OK to download.
STM32H7B3I DK >> Download of STM32H7B3I DK failed
STM32H7B3I Evulation >> Download 100%, OK
Internet is OK!
2023-02-17 1:07 AM
Can you provide screenshots please ? And also share the .log file located at C:\Users\USERNAME\AppData\Roaming\TouchGFX-4.21.1\TouchGFXDesigner.log.
Thanks,
/Yoann
2023-02-17 1:38 AM
2023-02-17 1:57 AM
Can you please try to create a project with STM32F746G-DISCO ? And let me know how it goes.
/Yoann
2023-02-17 2:03 AM
It went well to create a project with STM32F746G-DISCO
/Stefan
2023-02-17 2:17 AM
Then close TouchGFXDesigner, go to "C:\Users\USERNAME\AppData\Roaming", and delete the TouchGFX-4.21.1 folder. After that open TouchGFXDesigner 4.21.1 again, wait 1-2 minutes and try again with H7B3-DK.
2023-02-17 2:24 AM
Still problem downloading project STM32H7B3I DK after I followed your instructions.
/Stefan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.