cancel
Showing results for 
Search instead for 
Did you mean: 

Display jitters and object skewing

SAnve
Associate II

Hi TouchGFX Team,

  I am currently integrating TouchGFX on STM32F746NE custom board with TFT display of 800x480 resolution . I am using 24bit color depth. Currently facing two issues

1. I see lot of jitters on screen when there is a screen update. I could avoid by increasing VSYNC and Vertical Porch timings. But that resulted in lower refresh rate and caused screen flickering. Is there a way in TouchGFX to use additional buffers to draw and avoid such jitters ?

2. Second issue is object skewing, object appears perfectly fine on TouchGFX designer , but downloaded objects are skewed on y axis. What could be the root cause and How can I avoid this ?

Please let me know

Thanks & Best Regards,

Sanjay

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Martin KJELDSEN
Chief III

Hi @SAnve​,

  1. Yes, you can use single or double buffering. Please see HAL::setFrameBufferStartAddresses().
  2. Please show me some example of this. Sounds like porch setting issue.

/Martin

SAnve
Associate II

Hi Martin,

Thanks for your response.

  1. Currently I have enabled double buffering and animation storage

Below are source code lines

hal.setFrameBufferStartAddress((uint16_t*)frameBuf0, bitDepth, true, true);

I had to enable following settings to get rid of jitters on the screen

hal.setFrameRateCompensation(true);

hal.lockDMAToFront Porch(true);

I suspect that before framebuffer update is complete it is used for updating display. Only reducing VSYNC, VBP and VFP values avoids jitters, but it introduces flicker due to reduced refresh rate. Please let me know your input to overcome this issue.

2. Please find attached file, where you can see clock dial is skewed on y-axis.

Thanks & Best Regards,

Sanjay

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.