2019-09-19 5:59 AM
Hello,
I have a display issue when I using the wildcard buffer.
I already used wildcard buffer by the past on a previous version of touch GFX.
I created a new project for a custom board and the problem is that I can't modify a text with the wildcard buffer.
See my function below :
void Screen1View::Button1clicked()
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "Bonjour");
textArea1.resizeToCurrentText();
textArea1.invalidate();
}On the screen the letters (B,o,n,j,o,u and r) seems to be all on the top of the others, all at the same position.
I made some tests and in another one, I obtained only few letters of the complete word "njo" for exemple.
I think I use touch GFX function as needed because as I said I already complete an application on a previous custom board.
The only one difference is that on the previous project I used IAR and for this new one I use Atollic.
I also tried to complete the buffer, char by char :
textArea1Buffer[0] = 'B';
textArea1Buffer[1] = 'o';
textArea1Buffer[2] = 'n';
textArea1Buffer[3] = 'j';The result is the same.
It looks to be an abnormal behaviour.
Could you help me ?
Thank you
Regards,
Alexis
Solved! Go to Solution.
2019-09-20 6:14 AM
Not sure what's wrong with your application, but i re-made your example in 4.10.0:
/Martin
2019-09-19 6:46 AM
How large is your buffer? it should be at least 8 chars long (bonjour is 7 and \0 is 1). it's probably not that but you code only shows 4 places.
2019-09-19 6:51 AM
My buffer has a size of 11
2019-09-19 6:59 AM
Hi @ALuca
Hope this will solve your issue.
2019-09-20 3:02 AM
Hi PBU,
Thank you for the answer, the problem stay the same with this solution.
2019-09-20 6:14 AM
Not sure what's wrong with your application, but i re-made your example in 4.10.0:
/Martin
2019-09-23 11:13 PM
Hello Martin,
Thank you for your answer ! I forgot to define wildcard range on this project...
After that all is OK..
Alexis
2019-09-23 11:51 PM
That's great, @ALuca.
Does it make sense now? Since you don't know at asset-generation time which glyphs you'll need (no static strings defined) you'll choose a range of potential glyphs. E.g. if you're showing a text-message (which can be completely random) from a phone you need at least the entire alphabet + other symbols.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.