2023-07-11 10:41 AM
Hello,
I'm programming the STM32U5A9JDK with a C project including TouchGFX.
While debugging in STM32CubeIDE, I got this issue:
If I pause the debug session after the TouchGFX init, I wait about one minute and the debug session crash: the board does no more communicate and the console print "Target is not responding, retrying". I have to stop the debug session and reconnect the board to restart the debugging.
I only got this issue when TouchGFX init is added in my project and I checked in the register window that watchdog timers are stop in debug mode.
I don't see what's going on with my TouchGFX init, can I get help on this?
Thanks,
Thomas
Solved! Go to Solution.
2023-07-12 8:07 AM
I finally solve this issue by using an external st link v2 and stop using the embedded st link.
2023-07-12 8:07 AM
I finally solve this issue by using an external st link v2 and stop using the embedded st link.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.