2019-04-03 10:38 PM
Hi,
I am working on DCMI interface of STM32f407VGT micro controller to connect external device(not camera).And i am trying to get data from external device using 8-bit parallel data lines and PIXCLK frequency as 6.3MHz. Also providing H SYNC and V SYNC Signals as Hardware Synchronization.Always i am getting data from external device(Parallel) but initial data is missing .So how can i get proper data from external device without losing initial data.
Here is my configuration and Initialization code.
//GPIO Configuration
/**DCMI GPIO Configuration
PE4 ------> DCMI_D4
PE5 ------> DCMI_D6
PE6 ------> DCMI_D7
PA4 ------> DCMI_HSYNC
PA6 ------> DCMI_PIXCK
PC6 ------> DCMI_D0
PC7 ------> DCMI_D1
PC8 ------> DCMI_D2
PC9 ------> DCMI_D3
PB6 ------> DCMI_D5
PB7 ------> DCMI_VSYNC
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
//DCMI Initialization
static void MX_DCMI_Init(void)
{
hdcmi.Instance = DCMI;
hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;
hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING;
hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW;
hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_HIGH;
hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME;
hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
hdcmi.Init.JPEGMode = DCMI_JPEG_DISABLE;
if (HAL_DCMI_Init(&hdcmi) != HAL_OK)
{
Error_Handler();
}
}
//DMA Initialization
hdma_dcmi.Instance = DMA2_Stream1;
hdma_dcmi.Init.Channel = DMA_CHANNEL_1;
hdma_dcmi.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_dcmi.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_dcmi.Init.MemInc = DMA_MINC_ENABLE;
hdma_dcmi.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_dcmi.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_dcmi.Init.Mode = DMA_NORMAL;
hdma_dcmi.Init.Priority = DMA_PRIORITY_HIGH;
hdma_dcmi.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_dcmi) != HAL_OK)
{
Error_Handler();
}
//MAIN CODE
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_DCMI_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_DCMI_Init();
/* USER CODE */
if(HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)pData, 512)!= HAL_OK)
{
Error_Handler();
}
while (1)
{
if(DataRecieved)
{
DataRecieved = 0;
}
}
}
/**
* @User Callback (peripheral_ Memory transfer complete)
* @retval None
*/
void XfercmpltcallBack(DCMI_HandleTypeDef *hdcmi)
{
if(hdcmi->Instance == DCMI)
{
if(HAL_DCMI_Start_DMA(hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)pData, 512) != HAL_OK)
{
Error_Handler();
}
DataRecieved++;
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 50;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
2019-04-04 12:50 AM
How many frames of data do you lose and how do you flag to the device that you're ready to accept data?
2019-04-04 1:57 AM
Only last 4-bits of data i am losing in initial frame.
Here for the first time i am enabling capture bit (DCMI_CR Register) so it captures data from external device and it performs memory transfer operation after that if memory transfer is done than i am again enabling capture bit using user callback function (XfercmpltcallBack(hdcmi) ).
hdcmi->Instance->CR |= DCMI_CR_CAPTURE;
/**
* @brief DMA conversion complete callback.
* @param hdma pointer to a DMA_HandleTypeDef structure that contains
* the configuration information for the specified DMA module.
* @retval None
*/
static void DCMI_DMAXferCplt(DMA_HandleTypeDef *hdma)
{
uint32_t tmp = 0U;
DCMI_HandleTypeDef* hdcmi = ( DCMI_HandleTypeDef* )((DMA_HandleTypeDef* )hdma)->Parent;
if(hdcmi->XferCount != 0U)
{
/* Update memory 0 address location */
tmp = ((hdcmi->DMA_Handle->Instance->CR) & DMA_SxCR_CT);
if(((hdcmi->XferCount % 2U) == 0U) && (tmp != 0U))
{
tmp = hdcmi->DMA_Handle->Instance->M0AR;
HAL_DMAEx_ChangeMemory(hdcmi->DMA_Handle, (tmp + (8U*hdcmi->XferSize)), MEMORY0);
hdcmi->XferCount--;
}
/* Update memory 1 address location */
else if((hdcmi->DMA_Handle->Instance->CR & DMA_SxCR_CT) == 0U)
{
tmp = hdcmi->DMA_Handle->Instance->M1AR;
HAL_DMAEx_ChangeMemory(hdcmi->DMA_Handle, (tmp + (8U*hdcmi->XferSize)), MEMORY1);
hdcmi->XferCount--;
}
}
/* Update memory 0 address location */
else if((hdcmi->DMA_Handle->Instance->CR & DMA_SxCR_CT) != 0U)
{
hdcmi->DMA_Handle->Instance->M0AR = hdcmi->pBuffPtr;
}
/* Update memory 1 address location */
else if((hdcmi->DMA_Handle->Instance->CR & DMA_SxCR_CT) == 0U)
{
tmp = hdcmi->pBuffPtr;
hdcmi->DMA_Handle->Instance->M1AR = (tmp + (4U*hdcmi->XferSize));
hdcmi->XferCount = hdcmi->XferTransferNumber;
}
/* Check if the frame is transferred */
if(hdcmi->XferCount == hdcmi->XferTransferNumber)
{
/* Enable the Frame interrupt */
__HAL_DCMI_ENABLE_IT(hdcmi, DCMI_IT_FRAME);
/* When snapshot mode, set dcmi state to ready */
if((hdcmi->Instance->CR & DCMI_CR_CM) == DCMI_MODE_SNAPSHOT)
{
hdcmi->State= HAL_DCMI_STATE_READY;
}
/* User callback after Frame interrupt(transferred) */
if(DCMI_IT_FRAME)
{
XfercmpltcallBack(hdcmi);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.