2019-03-22 9:37 PM
I'm working on a custom board, where I'm introducing new features and testing each individually.
Example:
LTDC with the cubemx interface. Tested the operation. OK.
FMC with the cubemx interface. Tested the operation. OK.
DMA2D with the cubemx interface. Tested the operation. OK.
In short, I have to create each configuration separately, and the worst individually for each pin, because many pins appear set by default in CubeMX.
And there is a detail that I do not understand!
Why can not I copy all libraries when I'm in TrueSTUDIO, but when in MKD can I?
Since TrueSTUDIO is from ST, can not I manually configure my projects?
As I have an Eastern origin, I will patiently wait for software developers, contractors and CubeMX managers, "to graduate in the Faculty of Software Engineering, to explain this lesson I lost, I apologize for being an absent and inattentive student. "
Ivan Braga
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.