2023-02-21 4:42 AM
Hello,
I upgraded my project from version 4.16.1 to 4.21.1, and after re-generating the project in the touchgfx editor and copying all libjpeg files (includes and libs) from a demo project that uses a video in the folder Middlewares\ST\TouchGFX\touchgfx\3rdparty\libjpeg, and after adding all required paths in VS for the project to link correctly, I got this error when I run the project in VS : Code execution can't continue because libjpeg-8.dll was not found. This problem can be solved by reinstalling the software (which software are they talking about?!)
The libjpeg-8.dll file however is in the lib directory, next to the .libjpeg-8.a and libjpeg-8.lib
Any help would be more than welcomed as I've no idea how to solve this problem.
Thanks.
2023-02-22 2:09 AM
Hello GMeur,
Does your application run on simulator when you press F5 in TouchGFX Designer.
Have you checked if the paths for this lib are correct in the makefile and in the target file ?
(MyApplication\TouchGFX\generated\simulator\gcc\Makefile and MyApplication\TouchGFX\generated\simulator\msvs\touchgfx_prebuild.targets)
/Osman
2023-02-23 6:02 PM
I suppose you are not using STM32CubeMX since you are manually copy pasting the middleware folder? You run the project in VS with gcc/ a makefile (not accustomed to that way of working sorry)?
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.