2019-11-27 11:12 AM
Hi
Is there any way to change an object "z-order" via code?
Using the designer is easy, just click the button "Send backwards" and "Bring forward", this basically change in the "ViewBase.cpp" the order of adding the object to the screen.
Is there any way to do this after, for any object we add (in "setupScreen" function)?
Use Case: I have a page with some buttons to perform some actions, but would like that if the user press anywhere on the screen (that is not a button) to execute an action (change page), for that i am using a touchArea that i have to add manually, but since it is always the last object added it stays in front of other objects and captures the click for the buttons.
Thank You
Solved! Go to Solution.
2019-11-27 11:45 AM
Hi,
Just call remove(windget_you_want_in_front) and add this widget again with add(windget_you_want_in_front)
Sébastien
2019-11-27 11:45 AM
Hi,
Just call remove(windget_you_want_in_front) and add this widget again with add(windget_you_want_in_front)
Sébastien
2019-11-27 12:16 PM
Hi
thanks for the tip... yeah, simple and it works.
Just need to remember if i add more objects in the designer to update the function to remove them and add them after the toucharea.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.