2024-10-12 4:21 AM
hello friends
My program does not run! It stays on the initial startup screen.
I have reinstalled the program several times, but it did not fix it.
Can you give me some advice?
2024-10-12 6:29 AM
Maybe try this
2024-10-13 4:46 AM
Hello @Salar1993 ,
Did you try to install the latest release TouchGFX DESIGNER (v 4.24.1)?
Is this issue was also faced with latest release ?
Which Windows version do have on your PC?
If possible, share the log file that contains the message and steps when you use the tool, during TouchGFX Designer startup, connection to servers.
The logs of TouchGFX Designer are contained inside C:\Users\username\AppData\Roaming\TouchGFX-<version>\TouchGFXDesigner.log.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.