2020-06-03 9:32 PM
Hi Guys,
I want to connect 8" to 10" TFT LCD + Capacitive Touch Screen display with MIPI DSI interface to STM32F469I-Discovery just by removing the existing 4" TFT LCD. I had searched in the internet and I didn't get any TFT LCD CTP with MIPI DSI interface which can be directly connect to STM32F469I-Discovery board. STM32F469I-Discovery board uses 25 pin connector (CN10) for LCD and 6 pin connector (CN2) for Capacitive Touch screen.
Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?
With Regards
SUNIL K S
Ace Designers Ltd
2020-06-05 4:39 AM
Hi,
Thanks for the suggestion.
With Regards
Sunil K S
2020-06-05 5:04 AM
Hi,
I have ordered TFT LCD PH720128T003-ZBC02. I plan to connect with STM32MP1 (module VisionSOM-STM32MP1 company SOMLabs) https://somlabs.com/product/visionsom-stm32mp1/. I have also plan to connect with STM32F769 or STM32H74x.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.