2021-05-08 10:06 PM
The field DMA_Handle of the local data pointer phdcmi, which points to a global struct variable hDcmiEval, is not initialized in the function BSP_CAMERA_Init (from the file STM32Cube_FW_F4_V1.25.0/Drivers/BSP/STM32469I_EVAL/stm32469i_eval_camera.c).
uint8_t BSP_CAMERA_Init(uint32_t Resolution)
{
DCMI_HandleTypeDef *phdcmi;
uint8_t status = CAMERA_ERROR;
/* Get the DCMI handle structure */
phdcmi = &hDcmiEval;
/*** Configures the DCMI to interface with the camera module ***/
/* DCMI configuration */
phdcmi->Init.CaptureRate = DCMI_CR_ALL_FRAME;
phdcmi->Init.HSPolarity = DCMI_HSPOLARITY_HIGH;
phdcmi->Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;
phdcmi->Init.VSPolarity = DCMI_VSPOLARITY_HIGH;
phdcmi->Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
phdcmi->Init.PCKPolarity = DCMI_PCKPOLARITY_RISING;
phdcmi->Instance = DCMI;
/* Configure IO functionalities for CAMERA detect pin */
BSP_IO_Init();
/* Apply Camera Module hardware reset */
BSP_CAMERA_HwReset();
...
}In the function HAL_DCMI_Start_DMA (from the file STM32Cube_FW_F4_V1.25.0/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dcmi.c), the DMA_Handle field is used to store function pointers.
HAL_StatusTypeDef HAL_DCMI_Start_DMA(DCMI_HandleTypeDef* hdcmi, uint32_t DCMI_Mode, uint32_t pData, uint32_t Length)
{
/* Initialize the second memory address */
uint32_t SecondMemAddress = 0U;
/* Check function parameters */
assert_param(IS_DCMI_CAPTURE_MODE(DCMI_Mode));
/* Process Locked */
__HAL_LOCK(hdcmi);
/* Lock the DCMI peripheral state */
hdcmi->State = HAL_DCMI_STATE_BUSY;
/* Enable DCMI by setting DCMIEN bit */
__HAL_DCMI_ENABLE(hdcmi);
/* Configure the DCMI Mode */
hdcmi->Instance->CR &= ~(DCMI_CR_CM);
hdcmi->Instance->CR |= (uint32_t)(DCMI_Mode);
/* Set the DMA memory0 conversion complete callback */
hdcmi->DMA_Handle->XferCpltCallback = DCMI_DMAXferCplt;
/* Set the DMA error callback */
hdcmi->DMA_Handle->XferErrorCallback = DCMI_DMAError;
/* Set the dma abort callback */
hdcmi->DMA_Handle->XferAbortCallback = NULL;
...
}However, DMA_Handle points to the memory address 0x0000_0000, which is a invalid memory address.
In ARM Cortex-M4 MCUs, the code starts 0x800_0000.
I am confused why this application runs well and does not crash. Is address 0x0000_0000 a valid memory address?
2021-05-09 8:12 PM
The Camera_to_USBDisk application I use is in STM32F469I-EVAL, which belongs to STM32Cube_FW_F4_V1.25.0.
Does anybody can fix this bug?
2021-05-18 9:27 AM
Hello @Spencer_0 ,
Let me first welcome you to the STM32 Community :)
I added the adequate topics to your question in order to increase its chance to be reviewed by our experts.
Hello @Walid ZRELLI ,
Can you please have a look at this post and confirm this issue ?
Thanks
Imen
2021-05-19 1:40 AM
Hello @Spencer_0 ,
In case of using DCMI_DOUBLE_BUFFER mode, the second memory address will be updated as follows:
SecondMemAddress = (uint32_t)(pData + (4U*hdcmi->XferSize)) ;
You could check the HAL_DCMI_Start_DMA() funtion.
So, there is no bug to fix.
With Regards,
Walid.
2021-05-21 1:45 AM
Hello @Walid ZRELLI , thanks for your reply.
I use the gdb to debug the application, and I find that the application doesn't use the DCMI_DOUBLE_BUFFER mode in my case.
The execution trace is here:
#0 HAL_DCMI_Start_DMA (hdcmi=0x200020e4 <hDcmiEval>, DCMI_Mode=0x0, pData=0xc0177000, Length=0x2580) at ../../../Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dcmi.c:385
/* The program does not take the branch that uses the DCMI_DOUBLE_BUFFER mode here */
#1 0x0801012a in BSP_CAMERA_ContinuousStart (buff=0xc0177000 "\265\372\200") at ../../../Drivers/BSP/STM32469I_EVAL/stm32469i_eval_camera.c:276
#2 0x0802f15a in Camera_Init () at ../../Src/main.c:288
#3 0x0802f762 in main () at ../../Src/main.c:354Apparently, if the application doesn't use the DCMI_DOUBLE_BUFFER mode, the address is still not transformed, and the pointer`hdcmi->DMA_Handle` points to the address 0x0000_0000.
So I believe that it is still an uninitialized field bug.
However, the picture captured by the Camera is always blank in my case. I wonder that if the proper execution flow should take the DCMI_DOUBLE_BUFFER mode branch. Otherwise the image captured by the camera is blank.
With kind regards,
Spencer Zhou
2021-05-21 1:50 AM
Thanks for your help @Imen DAHMEN :grinning_face:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.