2020-11-09 5:35 AM
Hello !
With my TouchGFX designer, the digital widget and the analog clock widget do not work with the STM32G071 application template (at least with the simulator, I can not confirm with the board).
When I say it does not work I mean it is well displayed but the value (or animation) is never updated. The widget is frozen to the original value.
Solved! Go to Solution.
2021-03-15 4:05 AM
Hello @Community member ,
I cannot select this reply as the best because it is was not my issue.
That's why you should have create a new post.
Anyway, this behaviour should be specified by ST I think because the solution is not obvious.
Simon
2021-03-15 5:11 AM
Hi,
I agree and we plan on documenting that. It is specific to the G0, and we wish to further optimize the TouchGFX footprint in order to have more space to store images in internal flash.
/Romain
2021-03-15 5:15 AM
Hi @Romain DIELEMAN ,
Thank you for this information ! Good to know.
Simon
2022-10-17 4:15 PM
I Recently worked on STM32F407VGT6 . The same Hands was not displaying with serial SPI flash. But it was working with internal flash. Adding more space to G071 or 407 Internal flash is not the solution. It could be helpful if we get the workaround to get it run from external flash.
2022-10-18 7:24 AM
Create new ticket is better, but your idea animate from external spi isnt cool.
Place image from external to ram image cache is one way. For low space L8 with alpha palette is optimal.
2024-02-20 3:51 AM
Thank you. I applied these setting and problem is solved for me. :thumbs_up::folded_hands:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.