STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! SDMMC Does not work with TouchGFX Application.

Hi,Iam using a STM32F746 DISCO Board to use SDMMC in a TOUCHGFX Application but Iam not able to get past if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK) function. It gives error here. Even If I comment this section and re...

SMour.2 by Associate III
  • 3234 Views
  • 5 replies
  • 0 kudos

getPixelData() Hardfault

I have a screen with only 1 line of text and I get a Hard Fault when I try to run it. I get the fault here at the glyph->dataOffset:const uint8_t* GeneratedFont::getPixelData(const GlyphNode* glyph) const{const uint8_t* const* table = (const uint8_t*...

beezybee by Associate II
  • 4481 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.