STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Cygwin Error after rebasing

Hi, I'm using the STM32F769I-Eval board and have come accross the same Cygwin error which a lot of people seem to have come across. After reading through multiple posts the best solution I have found was here to use 'editbin' to perform the rebase as...

rriddell_0-1742907147877.png
rriddell by Associate II
  • 1682 Views
  • 4 replies
  • 2 kudos

Changing Colors of Vector Images

Hello,I understand there's been a similar question asked and answered here: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-does-touchgfx-directly-change-the-color-of-the-picture-in/td-p/116908, but I'd really like to emphasize my desire ...

JAlbr.1 by Associate III
  • 1760 Views
  • 3 replies
  • 0 kudos

Resolved! Black screen with TouchGFX

I have just started using TouchGFX on an Stm32H7A3ZIQ Nucleo board. I managed to setup the LTDC correctly and am able to change the color of the screen, which makes me assume that the LTDC is setup correctly.After setting up TouchGFX with FreeRTOS, f...

DavidL__0-1742852938643.png DavidL__1-1742853015250.png DavidL__2-1742853056070.png DavidL__3-1742853200431.png
DavidL_ by Associate III
  • 1192 Views
  • 1 replies
  • 1 kudos

How to add X/Y line chart with multiple series

I have my own TouchGFX App running on STM32H747I-DISCO board. It reads data from popular BME280 sensor chip via I2C interface. Now I need to show the "history" of measured temperature, pressure and humidity on a graph underneath the RTC date, day of ...

Louie88 by Senior II
  • 1185 Views
  • 1 replies
  • 0 kudos

Resolved! Tearing issue U599 DSI

I try implement 1424x280 DSI panel and it work, but transition on single buffer have trouble.I start with simple fadeout and attached video show result. Try off DCACHE ICACHE DMA2D GPU2D, no big difference. Exist example or recomm for video mode with...

MM..1 by Chief III
  • 1058 Views
  • 1 replies
  • 0 kudos

TFT LCD drivers for TouchGFX?

I am looking into using an STM32 with TouchGFX to drive a 2.4" TFT LCD. The LCD will have some type of internal driver (ILI9340/ILI9341/ST7789, etc). Are there drivers for these already? Or is this relatively standard (I doubt)? Or do I have to write...

NNar by Associate II
  • 10925 Views
  • 19 replies
  • 0 kudos

Question about GPU2D render speed

I use U599 driving a 480*480 lcd, there are two full screen texureMappers, two full screen cacheable containers. the first cacheable container rendered to dynamicBitmap1,the textureMapper1 use dynamicBitmap1 as source pic  . cacheable Container2 ( in...

amb by Senior
  • 2625 Views
  • 5 replies
  • 2 kudos

Resolved! Could any STMCU be used to drive dual LCD screens?

Hello Guys,I am searching for a MCU to drive dual LCD screens. Although I see some MCU (eg, STM32U5G9ZJTXQ) providing both DSI and RGB mode interfaces without pinout collision, I didn't see any description about whether the LTDC can output 2 differen...

srony by Associate II
  • 3826 Views
  • 7 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.