STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Shape-Widgets in TouchGFX?

The knowledge base text in widget->Circle shows 4 widgets (Box, Box with Border, Line and Circle) on the SHAPES, and the text indicates: "The Circle is located under Shapes in the TouchGFX Designer."Sorry, but, where is Shapes on the TouchGFX Desig...

DAmig by Associate II
  • 6246 Views
  • 15 replies
  • 0 kudos

Resolved! How do I determine which container is being pressed

To implement something like iconview in emwin,I created a​ Custom container,consist of a image and textarea. name as a icon.Then,create 2 screen .The screen1 use SwipeContainer ,whitch add 12 icon.Q1:How do I determine which icon is pressed?Q2:How do...

lxw by Senior
  • 1611 Views
  • 4 replies
  • 0 kudos

Problem with transitionCallback

Hi everyone,i enable touchgfx in my project starting with cubeMX.But it doen't run touchgfx.I use MDK-ARM5 with uKeil.In debug i see that after this instruction (inside gui_generated/common/FrontendApplicationBase.cpp)transitionCallback = touchgfx::C...

apll by Associate II
  • 615 Views
  • 0 replies
  • 0 kudos

Placing files in flash memory (json)

I'm trying to place a json file from my computer in qspi memory, to then read it. I'm not quite sure how to save the file on the board and then access it. Doing it on the simulator is easy but once I run the code on my stm32f769i-disc it crashes beca...

pmppires by Associate II
  • 2647 Views
  • 3 replies
  • 0 kudos

Latest STemWin version?

Hi,with my recent download of CubeMX I have got emWin version 5.44. Are there newer versions for the STM32F7 family? I would be interested in version 5.48 or higher because of the changed MENU widget function.RegardsJan

Jan1 by Associate II
  • 1392 Views
  • 1 replies
  • 1 kudos

Animation and single framebuffer

We want to use AnimationTextureMapper to animate an image and it works fine when we use doubble framebuffers but with a single framebuffer we get flickering. Because we have limited RAM I wonder if anyone has any ideas/tricks how to get flickerfree ...

MLind by Associate II
  • 1097 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.