STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Using Internal Flash Memory For Frame Buffer

I'm using the stm32f769i-disco1. Which has 2 mB of flash memory.https://www.st.com/en/evaluation-tools/32f769idiscovery.htmlI'm creating a very simply application that's drawing circles and squares and some text, so it's not using most of the flash. ...

Badam.17 by Associate II
  • 1551 Views
  • 2 replies
  • 0 kudos

cost and time for customize board

My project is customizing board with code to play file and run motors by those componentMicro controller stm32f4xx (or higher)USB connectionSt linker debuggerTouchscreen to select and play video filesAudio output circuit with audio amplifierSD card h...

amoha.8 by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

Draw Bitmap with "BSP_LCD_DrawBitmap" on STM32 F7

I'm experimenting with the LCD library on the STM32F746G-DISCO board. I wanted to display an image from a BMP file on the display. Unfortunately this never worked. I looked at several examples, and finally noticed that the function LL_ConvertLineToAR...

MMett by Associate III
  • 2759 Views
  • 2 replies
  • 0 kudos

3 bugs

1. TouchGFX Designer looks for ST-Link utility in:C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utilitywhile recent ST-Link version gets installed in:C:\Program Files (x86)\STM32 ST-LINK Utility\ST-LINK Utilityand different ...

TDJ by Lead
  • 12764 Views
  • 16 replies
  • 0 kudos

Resolved! Using separate Model for screens

Hi, Is it possible to use multiple models in touchgfx. I have designed six screens for my application and all the screens are interacting with a single model. I would like to use separate model for each of the screens. Is it possible to do that. I...

PBU by Associate III
  • 3007 Views
  • 6 replies
  • 0 kudos

Resolved! Change Font

Is there any way to change font of an application? I have a button that change the application style( buttons image ecc) but i need (graphic guy want) also to change the font, size and colout of the text. Is it that possible?

Zui by Senior
  • 3874 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.