STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32F4-DISCOVERY

I have a demo board STM32F429I-DISC1.There is a SPI configuration in LCD configuration function LCD_SPIConfig();And then void LCD_WriteData(uint8_t value) { /* Set WRX to send data */ LCD_CtrlLinesWrite(LCD_WRX_GPIO_PORT, LCD_WRX_PIN, Bit_SET);...

0690X000009YHVjQAO.png

Resolved! Images not displaying correctly

Hello ,In my project I am using many images as assets , some as a logo others just a background for a button.However, when I compile the project through Keil, the images appear weird and noisy.In the other hand when I compile the project through Touc...

0690X000009YFj5QAG.jpg 0690X000009YFj0QAG.jpg

Resolved! I need tips on editing Make file

Hi,I need to seperate my code into different .c and .h fileswhen I do this, the Keil IDE compile no problem. But the compiler from withing TouchGFX designer gives an error of undefined reference.I know this issue is solvable my editing the Make file ...

STM32CubeMX & STemWin

Posted on April 23, 2018 at 20:45Hi I am trying to create an interface with STemWin using cubeMX.I did everthing in [STM32CubeMX for STM32 configurationand initialization C code generation (UM1718 User manual)].[You can reach this file cubeMX app->D...

Cevdet by Associate III
  • 6223 Views
  • 16 replies
  • 0 kudos

TouchGFX using FileSystem on QSPI

Hello,I am evaluating TouchGFX and I read this :examples of memory types that are not memory mapped and thus require cachingAll NAND-based flashesSD cardsAnything with a file systemQuadSPI NOR if your microcontroller does not include memory-mapping f...

LGall by Associate II
  • 2540 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.