STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Integrating My own LCD to STM32F429ZI

I Have STM32F429ZI board which is working well with its inbuilt LCD board. I want to integrate my new LCD board from 3rd party. But when I connected the pins correctly and I turn on the board , the LCD board returns no response even the backlight is ...

NS.16 by Associate II
  • 815 Views
  • 0 replies
  • 0 kudos

How can I create interaction if the screens are having only custom containers without any buttons or others?

I am using few custom containers in all the screens I created. I want to make interaction that when i touch one custom container it should take me to that particular screen. But there is no option showing in Trigger. How can i make interaction if the...

YK.10 by Associate II
  • 2156 Views
  • 5 replies
  • 0 kudos

4.11 Can not create/open project

I check the log, it will pop this error:System.ArgumentException: 已添加了具有相�?�键的项。(An item with the same key has already been added)  在 System.ThrowHelper.ThrowArgumentException(ExceptionResource resource)  在 System.Collections.Generic.Dictionary`2.Ins...

DJin.3 by Associate
  • 952 Views
  • 1 replies
  • 0 kudos

TouchGFX 4.10.0 and MSVS 2019

I am new to coding in touchgfx. i am using touchgfx 4.10.0 version and microsoft visual studio 2019. Depends on version, is there any difference in coding method?I followed one button example, which was already available in touchgfx examples. I devel...

YK.10 by Associate II
  • 1055 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.