STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to interface mcufriend 2.4 tft LCD.

Hi ,I am trying to interface a touch scren lcd with stm32 board. I have an mcufriend 2.4" touch screen lcd and i intend to interface it with nucleo-f303re board. I ,unfortunately, am not able to find a datasheet for the lcd. I know that the lcd can b...

hp26 by Associate II
  • 3944 Views
  • 4 replies
  • 0 kudos

TouchGFX with custom Display

Hello,when I run the code with the STM32F769 discovery bord display, everything works fine.But when I use a differnt display the constructor for the start screen is not called from touch gfx lib. Does anybody know why this is only working with the di...

DPfei.16 by Associate III
  • 2183 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX + TouchGFX 'Error during code generation'

Hi,I'm trying to generate a new project for the STM32F469IDISCOVERY using CubeMX 5.2.0 and TouchGFX 4.10.0. All peripherals are initialized with the default modes. I use STM32CubeIDE as toolchain/IDE.After enabling the Graphics framework using TouchG...

Ade W by Associate II
  • 6041 Views
  • 12 replies
  • 0 kudos

Need help getting display to match TouchGFX simulator.

Trying to get a new display board working using STM32CubeIDE and TouchGFX. Processor is STM32F469BI, Display is an 800x480 with 24BPP RGB888 interface. I've also got a 128Mb x 32 external SDRAM for the frame buffer. I've gone through the data sheets ...

0690X00000A9j6HQAR.jpg 0690X00000A9j3NQAR.jpg
TSton by Associate II
  • 1242 Views
  • 1 replies
  • 0 kudos

STM32F7 LTDC and TIM2

If I configure the LTDC interface on my STM32F746IE device, TIM2 is disabled.I can reset the state of LTDC_R2 (PA1), then TIM2 is available, but disables itself after reconfiguring LTDC.PA0 = TIM2 CH1PA2 = TIM2 CH3I searched accros the datasheet, ref...

0690X00000A9goQQAR.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.