STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touchgfx visual studio compilation error "Severity Code Description Project File Line Suppression State Error LNK1104 cannot open file "

Hi !I am using touchgfx Version 4.10.0 and visual studio community 2019 version 16.0.4 and getting "Severity Code Description Project File Line Suppression StateError LNK1104 cannot open file '..\..\touchgfx\\lib\win\msvs\libtouchgfx_v142_debug.lib'...

Adding a rotating knob ?

Can I add a rotating knob ? If so , how ? Would it be possible to load a filmstrip ?I use that for VST plugins although I see no widgets for that ?Maybe the circle progress , somehow ?

STM32H753BI - HDMI + breakout boards

Hi Guys, I'll be starting new with the STM32H753BI and need to ask a few questions.1. Using the HDMI function on the MPU: Do I have to pay any royalties or anything else to use the HDMI interface in our own commercial product?2. Breakout board for th...

PAdam.6 by Associate II
  • 2048 Views
  • 4 replies
  • 0 kudos

TouchGFX designer "Generate Assets Error"?

I installed the STM32Cube related programs in the following order.And all programs are up to date.(1) STM32CubeMX(2) TrueStudio(3) STM32CubeProg(4) STMCubeL4(5) STM32CubeIDE(6) TouchGFX designerWhen I created a sample to test TouchGFX designer, but I...

JPark.14 by Associate III
  • 3541 Views
  • 7 replies
  • 0 kudos

touchgfx designer error during code generation

Converting imagesZip end of central directory signature not foundan error occurred in converting texts:Zip end of central directory signature not foundsimulator/gcc/Makefile:247: recipe for target 'generated/texts/include/texts/TextKeysAndLanguages.h...

zyu.364 by Associate
  • 1076 Views
  • 1 replies
  • 0 kudos

Problem: how get data of DCMI and stored in other memory (flash ic & sd card & etc.) without stored full data in internal sram?

hi everyone i use stm32f407vg, camera ov7725(equal with ov7670) and spi flash ic w25q128.now program working with HAl DCMI DMA for get data RGB565 of ov7725 and stored in sram and show in tft lcd but need to large memory.add spi flash ic for stored.P...

kshin.111 by Associate III
  • 1506 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.