STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Simulator in project upgrated to TouchGFX 4.13 won't work

Hej Hej,Since I upgrated my project from version 4.12 to 4.13, the simulator won't launch anymore (the project was initially created with TouchGFX 4.10). VS throws two error msgs :1) unresolved external symbols void __cdecl touchgfx::simulator_enable...

GMeur by Senior II
  • 2029 Views
  • 3 replies
  • 0 kudos

STM32F427 + TFT LCD + STemWIN?

Hello, I have a few questions about the subject.Suppose you use a display TFT with a controller any as ILI9341 or ST778 320x240 256k color 8bit interface or SPI. with STM32F427.The first question concerns how to connect the LCD to the MCULCD support ...

Berger1 by Associate
  • 1956 Views
  • 3 replies
  • 0 kudos

MIPI DSI_D2 &D3

HelloI bought an Stm32f769-disco board to evaluate the STM32F7 and I'd mike to go forward on my design...On the board you have a 4" Mipi Dsi display and I would like to implement a 7" mipi display.The problem that i found is that most ipi display on ...

PAMSA.1 by Associate
  • 760 Views
  • 0 replies
  • 1 kudos

CubeMX and Touchgfx with custom board

HI, I am using a custom board with STM32F429IGT, and 480X272 TFT screen which are wired to LTDC Pins . The TFT part number is K430WQA-V4-F.I built a Project using CubeMxVer 5.1 and Touchgfx Ver 4.1. Compiled and downloaded the code in the board after...

bindhawa by Associate II
  • 3947 Views
  • 9 replies
  • 0 kudos

Resolved! Touchgfx 4.13 and Cubemx 5.5 project creation

Hi,I use the .ioc file in STM32F746-DISCO v.3.0.0 project, import it to CUBE IDE and used the option to create a project form ioc file. But even i compiled and run in in stm32f746 board, nothing happens. Any reason for this, or whats the fix. My end ...

Cannot run target or simulator

Hello, I cannot run target nor run the simulator eventhough I can debug the solution file from VisualStudio. There are no errors in the VisualStudio. So what might be the reason behind that? Detailed Log is showing tons of errors and failures. Here i...

GunkutA by Senior
  • 1766 Views
  • 6 replies
  • 0 kudos

Resolved! Plans for a "Hello TouchGFX World" project tutorial?

I want to start with TouchGFX, but I see too much people in this forum struggling to do a basic project for a development boards from ST. I imagine how hard it should be a custom board.Has ST plans to release a basic step by step tutorial showing how...

Asantos by Senior
  • 4324 Views
  • 16 replies
  • 0 kudos

How can I get started with OV2640 camera module?

Hi!I have a STM32 F446RE Nucleo board and that bord have DCMI included.I wonder if I only need to connect the OV2640 camera module to the GPIO's of F446RE and then I'm done?Or do I need to write some more code?Where do I start?The only information I ...

0690X00000BwMFwQAN.png
DMårt by Lead
  • 4236 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.