STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Wavy pattern in 480x272 Resistive display

HiWe have used touchgfx design in our customized STM32F746G project and using same hardware design of STM32F746G discovery board.While running, some wavy pattern is appearing on screen.I have attached the video for your reference .We have used FREE ...

STM-User by Associate II
  • 1455 Views
  • 2 replies
  • 0 kudos

Resolved! LTDC absent in the multimedia category?

Hi,I am creating a project with TouchGFX graphics on STM32F412G-DISCO. I have already downloaded and installed XCUBE-TOUCHGFX 4.14 and it is visible in "additional software" category. When selecting driver, the LTDC is grayed out. (attached) It is al...

EJ.1 by Associate II
  • 1922 Views
  • 2 replies
  • 0 kudos

TouchGFX problem with shape element

Hello everyone!I have a STM32H7B3I-DK board.I use TouchGFX Designer ver 4.13.0 and created a simple project.The project consist of one screen with two elements: box1 & image1Also I created eclipse project with touchgfx framework, FreeRTOS and TouchGF...

OShan.1 by Associate
  • 1690 Views
  • 3 replies
  • 0 kudos

Add or Remove item from a Scroll List

Hi everyone,I've been working on a project with STM32 and touchGFX. I'm working with a 7 inch touchscreen display. In one screen, i inserted a scrollList. I'm getting to change it's items and manipulate the list at setupScreen and scrollListUpdateIte...

Why isn't project structure started from a TouchGFX Application Template the same as one started from Stm32CubeIDE?

I am asking this question in a new thread as I was hi-jacking another threadThe project structure displayed in Stm32CubeIDE's Project Explorer is quite different depending on where the project originated.When a project is created in Stm32CubeIDE (fro...

0693W000000WelaQAC.png 0693W000000Weo5QAC.png 0693W000000WepNQAS.png 0693W000000Weq1QAC.png
scottSD by Lead
  • 1133 Views
  • 1 replies
  • 0 kudos

TouchGFX Partial framebuffers, Example/Help?

Hi, I am using a Nucleo F401RE with ILI9341 LCD Display and Touchgfx. I have managed to get the display working with a single framebuffer but the RAM on the MCU isnt capible of handling the full screen size (320 x 240), so i will have to use partial ...

MikeP by Senior
  • 1102 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.