STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Running TouchGFX on STM32F2 series MCU

Hi,I need al little help running TouchGFX to a STM32F207VG MCU. We already have a custom board featuring this MCU and a touchscreen with an ILI9341 driver IC. The screen communication is done using the FSMC on the MCU. I've got code working to write ...

JBoec.1 by Associate II
  • 7075 Views
  • 12 replies
  • 0 kudos

Can't get a stable VGA output on Nucleo-H743ZI2 board.

I have connected LTDC output to VGA monitor input and the picture is flickering. I've connected HSYNC and VSYNC signals, ground pin and only the highest R/G/B bits over 500 Ohm resistors to R/G/B input signals of the monitor. I've set vertical/horizo...

Slina by Associate III
  • 983 Views
  • 0 replies
  • 0 kudos

STM32F413ZH TouchGFX configuration

Hello,I am trying to display something on the display of a STM32F413ZH board. Following the video in link below I have configured everything in CubeMX (hopefully correctly). Then, the video suggested to get some code for the memory init from an empty...

DDori.1 by Associate III
  • 721 Views
  • 0 replies
  • 0 kudos

Resolved! Merging two touchgfx project

Hello,We have a touchgfx project. I design main screens and write board specific codes to project. My colleauge design some other screens for same project . Is there any way to import his screens to my touchgfx project (with protecting my screens) ?...

Epamuk by Associate III
  • 2409 Views
  • 4 replies
  • 0 kudos

IOC file for STM32H7B3I-DK

Where can I find a IOC file for the STM32H7B3I-DK? As this is a ST supplied Discovery Kit, there should be a IOC file that includes all the CPU internal memory and external memories and GPIOs defined. CubeMX 1.8.0 and TouchGFX 4.15 generate different...

RScot.2 by Associate II
  • 1509 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.