STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How do I get click coordinates continuously?

Hello!I want to click on the touch screen, get the coordinates, then, without releasing my finger, move my finger and get new coordinates continuously.Like slider widget)How do I do this?This codevoid PRINT_PROGRESS_ScreenView::Box3DClickHandler(cons...

EEuge by Senior
  • 1460 Views
  • 3 replies
  • 0 kudos

How to get current videobufer (videopage)?

Hello!I have a 3D libray, which generates pixeldata.I didn't found functions or widgets, which allow to draw on it's canvas.So, I want to direct write image to memory.Like thisfor(uint16_t x = 0; x <= 700; x++) for(uint16_t y = 0; y <= 200; y++) ...

EEuge by Senior
  • 572 Views
  • 0 replies
  • 0 kudos

Error when updating while using dfu bootloader.

​I'm using the dfu bootloader, but I can't figure out the cause.​I entered the address value of the bootloader as well as the address value (0x08010000) of the application and the offset after viewing several posts.​It works if you proceed with the f...

Cwonh.1 by Associate
  • 1458 Views
  • 1 replies
  • 0 kudos

STemWIN does not work on STM32L4R9-DISCO

I'm trying to start the Hello World application and the application generates HardFalut when calling the function GUI_DispStringHCenterAt. While debugging it seem that within the library function GUI__GetLineDistX a call to null pointer function happ...

bkupev by Associate
  • 859 Views
  • 0 replies
  • 0 kudos

Resolved! About using variables in TouchGFX

folder is model ,main_page_screen, pw_touchgfxactivev_screen.​I want to use the variables A declared in the model in main_screen and pw_page_screen. I don't know how to declare variables and how to use them.​For example, variable A is declared in mod...

0693W000006I3BmQAK.png
PKunK.1 by Associate III
  • 4551 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.