STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

handleTickEvent enable and disable

I have an animation that the image is getting bigger by the tick. But I want that when it gets a "true" once from model , the animation gets started and continue until it gets a "false". void IgnitionOnDemoScreenView::ShowUpLogo(bool Logo, bool Fade)...

Ezgi by Senior
  • 1391 Views
  • 2 replies
  • 0 kudos

Resolved! No reaction to touch

Hey!I took the working project that is generated by TouchGFX Designer as a reference and made a new project on the DISCOVERY-F469 board.I made UI with two screens. Screen1 has a button to jump to screen 2 and an animated image.After flashing the boar...

VLau by Associate III
  • 3661 Views
  • 7 replies
  • 0 kudos

Resolved! Where can I find the source code of touchgfx library?

When I want to understand how touchgfx platform works, especially the operation on the framebuffer, I realize there are some functions I could not get the source code e.g. the functions swapFrameBuffers() and tick() below which seems to be defined in...

BParh.1 by Senior III
  • 3487 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.