STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! I want to display a variable string in a custom list

I am always indebted.I have a ListLayout in touchgfx template.The list shows his icon and a fixed string.I want to add a variable string to this.I want to display a variable string using "% d", "% f", "% s" of sprintf ().How should it be realized?A s...

Ebun.1 by Senior
  • 1880 Views
  • 2 replies
  • 0 kudos

Resolved! Fail to used L8 image

I used ImageMagick to change a image into 256 colors that I want to used L8_RGB565 image. magick convert ***.png  -colors 256 ***_L8.pngBut the TouchGFX compiler returned an error : ERROR: Too many colors (762) for palette. Consider using RGB56...

V.H by Senior
  • 2251 Views
  • 5 replies
  • 1 kudos

Resolved! How to detect long press on custom container?

So I create a simple custom container containing just a box. Then I create 3 instances of this custom container in Screen1. I modify the custom container class to detect single click. But how to detect long press > 1s on any of these 3 containers?Att...

BParh.1 by Senior III
  • 4251 Views
  • 8 replies
  • 0 kudos

Transfering and displaying large amount of variables

Hi, I would like to ask as I never saw any effective example, how could I effectively update a lot of information from backend to frontend.Lets assume I have 40 variables of difetent types for example uint16_t, int8_t, bool, is there any effective wa...

AFire.1 by Associate II
  • 1635 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.